Can vpu simultaneously decoding?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can vpu simultaneously decoding?

ソリューションへジャンプ
2,619件の閲覧回数
397028133
Contributor III

我在使用vpu进行视频编码的同时,使用vpu进行解码视频,这样可以吗?

0 件の賞賛
返信
1 解決策
2,537件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xiaogang

Q: I use vpu for video coding at the same time, the use of video decoding vpu, this can?

A: simultaneous encoding and decoding is possible, please check presentation on

https://community.nxp.com/thread/439241

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,538件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xiaogang

Q: I use vpu for video coding at the same time, the use of video decoding vpu, this can?

A: simultaneous encoding and decoding is possible, please check presentation on

https://community.nxp.com/thread/439241

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,537件の閲覧回数
397028133
Contributor III

Hi igorpadykov

  Thank you for your answer,I did it.

0 件の賞賛
返信