Can vpu simultaneously decoding?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can vpu simultaneously decoding?

Jump to solution
2,622 Views
397028133
Contributor III

我在使用vpu进行视频编码的同时,使用vpu进行解码视频,这样可以吗?

0 Kudos
Reply
1 Solution
2,540 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xiaogang

Q: I use vpu for video coding at the same time, the use of video decoding vpu, this can?

A: simultaneous encoding and decoding is possible, please check presentation on

https://community.nxp.com/thread/439241

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,541 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xiaogang

Q: I use vpu for video coding at the same time, the use of video decoding vpu, this can?

A: simultaneous encoding and decoding is possible, please check presentation on

https://community.nxp.com/thread/439241

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,540 Views
397028133
Contributor III

Hi igorpadykov

  Thank you for your answer,I did it.

0 Kudos
Reply