Can the 8MIC-RPI-MX8 be used with Android?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can the 8MIC-RPI-MX8 be used with Android?

1,687件の閲覧回数
anurag16doshi
Contributor III

I have procured 8MIC-RPI-MX8 and want to use it to record audio on the imx8 Nano EVK board. I followed the getting started guide for the device but the mics could not pick any audio up. I think that it is because the mic does not run with Android on the chip. do you think this is true?

If not why do you think the mics are not picking up any sound?

Can someone also provide ways to run the mic with Android if they have tried working with it?

 

TIA,

Anurag

0 件の賞賛
返信
2 返答(返信)

1,671件の閲覧回数
art
NXP Employee
NXP Employee

The 8MIC-RPI-MX8 board uses the PDM microphones and PDM interface of the i.MX8MMini/Nano processors, that is not supported by Android. Only regular SAI interface is supported by Android.

Best Regards,
Artur

0 件の賞賛
返信

1,665件の閲覧回数
anurag16doshi
Contributor III

Hey.

The solution to use this I found was to take out the R24 resistor on the MIC. This is connected to the mute button on the MIC and this made the mics on the extension appear mute. After removing this I found that the mics pic up audio and record as well. Thanks for your help though.

0 件の賞賛
返信