Can the 8MIC-RPI-MX8 be used with Android?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can the 8MIC-RPI-MX8 be used with Android?

1,714 Views
anurag16doshi
Contributor II

I have procured 8MIC-RPI-MX8 and want to use it to record audio on the imx8 Nano EVK board. I followed the getting started guide for the device but the mics could not pick any audio up. I think that it is because the mic does not run with Android on the chip. do you think this is true?

If not why do you think the mics are not picking up any sound?

Can someone also provide ways to run the mic with Android if they have tried working with it?

 

TIA,

Anurag

0 Kudos
Reply
2 Replies

1,698 Views
art
NXP Employee
NXP Employee

The 8MIC-RPI-MX8 board uses the PDM microphones and PDM interface of the i.MX8MMini/Nano processors, that is not supported by Android. Only regular SAI interface is supported by Android.

Best Regards,
Artur

0 Kudos
Reply

1,692 Views
anurag16doshi
Contributor II

Hey.

The solution to use this I found was to take out the R24 resistor on the MIC. This is connected to the mute button on the MIC and this made the mics on the extension appear mute. After removing this I found that the mics pic up audio and record as well. Thanks for your help though.

0 Kudos
Reply