Can't open camera with OpenCV

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't open camera with OpenCV

1,557件の閲覧回数
zhiyuan_song
Contributor II

I tried some basic example code to get a picture from my camera with OpenCV, but all I get is the following error:

VIDEOIO ERROR: libv4l unable to ioctl S_FMT
VIDEOIO ERROR: libv4l unable to ioctl VIDIOCSPICT

why?

camera:ov5640 or mipi ov5640

Development board:imx6q

0 件の賞賛
返信
1 返信

1,482件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello song,

Error may be caused by i2c errors, one can debug it with oscilloscope in ov5640 I2C probe function ov5640_probe() or similar if other sensor was used

ov5640.c\capture\mxc\platform\media\drivers - linux-imx - i.MX Linux kernel 

You can debug it using AN4553 Using Open Source Debugging

Tools for Linux on i.MX Processors
https://www.nxp.com/docs/en/application-note/AN4553.pdf

0 件の賞賛
返信