Can't login on Ubuntu rootfs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't login on Ubuntu rootfs

1,304 Views
erikraynolds
Contributor IV

Per https://community.nxp.com/docs/DOC-330147 I've installed Ubuntu rootfs. Unfortunately can't login. I do have "login screen" and got stuck on this screen. Is it possible to login directly without login screen (automatic login)?

Today I can't login through "login screen" either as root, or as via created user L:MyUser P:MyUser .

Does anybody have experience login with it?

Thank you.

0 Kudos
Reply
1 Reply

1,112 Views
b36401
NXP Employee
NXP Employee

If there is some issue with logging without password I can suggest to try to set some password for root instead:
passwd -R /media/rootfs/ root

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply