Can't load u-boot with MfgTool on our custom Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't load u-boot with MfgTool on our custom Board

804 次查看
francoisrey
Contributor III

Hi,

I have received our custom board based on sabrelite design.

I try to run u-boot on it with MfgTool but it failed with the following error :

Reason is unknown, failed to run command: type="boot" body="Recovery" file="u-boot-mx6q-sabrelite.bin" timeout="10" onError="" text="Loading uboot." Descripteur non valide

Perhaps it's a hardware bug, but I have check all the schematic, all voltages, all oscillator and I didn't find any error.

Anyone have an idea ?

标签 (1)
0 项奖励
回复
0 回复数