Hello
I am working on imx-4.14.98-2.0.0_ga for RCU porting with lirc.
Follow the below steps to build image
DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source fsl-setup-release.sh -b build-wayland
bitbake fsl-image-multimedia-full
I also append
IMAGE_INSTALL_append = " \
lirc \
v4l-utils \
"
in local.conf
And in "/tmp/work/aarch64-mx8mm-poky-linux/v4l-utils/1.12.3-r0/image/usr/bin", I can see those files.
cec-compliance
cec-follower
decode_tm6000
dvb-format-convert
dvbv5-scan
ir-ctl
ivtv-ctl
rds-ctl
v4l2-ctl
cec-ctl
cx18-ctl
dvb-fe-tool
dvbv5-daemon
dvbv5-zap
ir-keytable
media-ctl
v4l2-compliance
v4l2-sysfs-path
Some files are presented in the rootfs of i.mx8mm platform (kernel mode), but some files are not.
Can someone help me to resolve this problem?
Thanks.
Julius
for v4l-utils look yocto/meta-openembedded/meta-oe/recipes-multimedia/v4l2apps/v4l-utils_<version>.bb
Hi Igor
Thanks your feedback.
Unfortunately, it is no helpful for us.
We knew how to create customer layer and create application like "hello world" and build-in rootfs.
In case, we hope you can help to advise where the meta layer define to decide the lirc part.
Thanks.
Hi juliuswu
one can look at below guidelines how to add and test custom package
Best regards
igor