Can't build Android Things images

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't build Android Things images

Jump to solution
1,657 Views
stefanosanna
Contributor I

Following the instructions in the PICO-i MX6UL-QSG.pdf document, I'm not able to self-build the Android Things images for the PICO board. More precisely, the command "lunch iot_imx6ul_pico-eng" fails because the "iot_imx6ul_pico-eng" configuration does not exist. Probably it needs a different bootloader, I was unable to find it. Where may I find update information on this topic?

Thank you.

Stefano.

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
1,200 Views
robertthompsons
NXP Employee
NXP Employee

Do to a last minute change by Google the source for Android Things will not be pushed to the AOSP until code is production ready. Based on this currently only the binary image is available from System Image Downloads | Android Things 

The updated docs can be found at: Android Things with i.MX 6UL|NXP 

View solution in original post

0 Kudos
Reply
1 Reply
1,201 Views
robertthompsons
NXP Employee
NXP Employee

Do to a last minute change by Google the source for Android Things will not be pushed to the AOSP until code is production ready. Based on this currently only the binary image is available from System Image Downloads | Android Things 

The updated docs can be found at: Android Things with i.MX 6UL|NXP 

0 Kudos
Reply