Can't boot from Android demo image on i.MX53QSB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't boot from Android demo image on i.MX53QSB

2,000 次查看
HenryChiang
Contributor I

Hi

I download Android demo image version 4.1 from http://www.adeneo-embedded.com/Products/Board-Support-Packages/Freescale

I follow “Adeneo i.MX53 Quick Start Board BSP for Android Gingerbread v4.1 User Guide and Release Notes” to install and build Android.

But it will boot hang and fail as follow.
Would someone please help it?

Thanks

The follow is log from UART

*********************************************************************************************************

U-Boot 2009.08-00322-g6450ddc-dirty (Jan 03 2012 - 15:01:45)

CPU:   Freescale i.MX53 family 2.1V at 800 MHz
mx53 pll1: 800MHz
mx53 pll2: 400MHz
mx53 pll3: 216MHz
mx53 pll4: 455MHz
ipg clock     : 66666666Hz
ipg per clock : 33333333Hz
uart clock    : 66666666Hz
cspi clock    : 54000000Hz
ahb clock     : 133333333Hz
axi_a clock   : 400000000Hz
axi_b clock   : 200000000Hz
emi_slow clock: 133333333Hz
ddr clock     : 400000000Hz
esdhc1 clock  : 80000000Hz
esdhc2 clock  : 80000000Hz
esdhc3 clock  : 80000000Hz
esdhc4 clock  : 80000000Hz
nfc clock     : 26666666Hz
Board: MX53-LOCO 1.0
Boot Reason: [POR]
Boot Device: SD
I2C:   ready
DRAM:   1 GB
MMC:   FSL_ESDHC: 0, FSL_ESDHC: 1
In:    serial
Out:   serial
Err:   serial
da9052_i2c_is_connected - i2c write success....
Serial reinitilized!
Checking for recovery command file...
Net:   got MAC address from IIM: 00:04:9f:01:b4:f9
FEC0 [PRIME]
Hit any key to stop autoboot:  0

MMC read: dev # 0, block # 2048, count 8192 partition # 0 ...
8192 blocks read: OK

MMC read: dev # 0, block # 12288, count 768 partition # 0 ...
768 blocks read: OK
## Booting kernel from Legacy Image at 70800000 ...
   Image Name:   Linux-2.6.35.3-01162-gd0d6a6d-di
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    3325172 Bytes =  3.2 MB
   Load Address: 70008000
   Entry Point:  70008000
   Verifying Checksum ... OK
## Loading init Ramdisk from Legacy Image at 70d00000 ...
   Image Name:   Android Root Filesystem
   Image Type:   ARM Linux RAMDisk Image (uncompressed)
   Data Size:    182026 Bytes = 177.8 kB
   Load Address: 70308000
   Entry Point:  70308000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Initializing cgroup subsys cpu
Linux version 2.6.35.3-01162-gd0d6a6d-dirty (marvell@marvell-desktop) (gcc versi
on 4.4.3 (GCC) ) #7 PREEMPT Tue Jan 3 15:03:12 CST 2012
CPU: ARMv7 Processor [412fc085] revision 5 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache
Machine: Freescale MX53 LOCO Board
Memory policy: ECC disabled, Data cache writeback
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 234496
Kernel command line: console=ttymxc0,115200 di0_primary calibration init=/init a
ndroidboot.console=ttymxc0
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
allocated 7864320 bytes of page_cgroup
please try 'cgroup_disable=memory' option if you don't want memory cgroups
Memory: 416MB 512MB = 928MB total
Memory: 924204k/924204k available, 26068k reserved, 0K highmem
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    DMA     : 0xf9e00000 - 0xffe00000   (  96 MB)
    vmalloc : 0xe0800000 - 0xf4000000   ( 312 MB)
    lowmem  : 0x80000000 - 0xe0000000   (1536 MB)
    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)
    modules : 0x7f000000 - 0x7fe00000   (  14 MB)
      .init : 0x80008000 - 0x80039000   ( 196 kB)
      .text : 0x80039000 - 0x80892000   (8548 kB)
      .data : 0x808b2000 - 0x8091b6c0   ( 422 kB)
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
        RCU-based detection of stalled CPUs is disabled.
        Verbose stalled-CPUs detection is disabled.
NR_IRQS:368
MXC GPIO hardware
MXC IRQ initialized
MXC_Early serial console at MMIO 0x53fbc000 (options '115200')
bootconsole [ttymxc0] enabled
Console: colour dummy device 80x30
Calibrating delay loop... 999.42 BogoMIPS (lpj=4997120)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
Initializing cgroup subsys debug
Initializing cgroup subsys ns
Initializing cgroup subsys cpuacct
Initializing cgroup subsys memory
Initializing cgroup subsys devices
Initializing cgroup subsys freezer
Initializing cgroup subsys blkio
CPU: Testing write buffer coherency: ok
regulator: core version 0.5
NET: Registered protocol family 16
i.MX IRAM pool: 128 KB@0xe0840000
IRAM READY
CPU is i.MX53 Revision 2.1
Using SDMA I.API
MXC DMA API initialized
IMX usb wakeup probe
IMX usb wakeup probe
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
da9052_i2c_is_connected - i2c read success....
regulator: DA9052_LDO1: 600 <--> 1800 mV at 1300 mV normal
regulator: DA9052_LDO2: 600 <--> 1800 mV at 1300 mV normal
regulator: DA9052_LDO3: 1725 <--> 3300 mV at 3300 mV normal
regulator: DA9052_LDO4: 1725 <--> 3300 mV at 2775 mV normal
regulator: DA9052_LDO5: 1200 <--> 3600 mV at 1300 mV normal
regulator: DA9052_LDO6: 1200 <--> 3600 mV at 1300 mV normal
regulator: DA9052_LDO7: 1200 <--> 3600 mV at 2750 mV normal
regulator: DA9052_LDO8: 1200 <--> 3600 mV at 1800 mV normal
regulator: DA9052_LDO9: 1250 <--> 3650 mV at 1500 mV normal
regulator: DA9052_LDO10: 1200 <--> 3600 mV at 1300 mV normal
regulator: DA9052_BUCK_CORE: 500 <--> 2075 mV at 1250 mV normal
regulator: DA9052_BUCK_PRO: 500 <--> 2075 mV at 1300 mV normal
regulator: DA9052_BUCK_MEM: 925 <--> 2500 mV at 1500 mV normal
regulator: DA9052_BUCK_PERI: 1800 <--> 3600 mV at 3600 mV normal
DA9053 chip ID reg read=0xa3
BB version probed
IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
Advanced Linux Sound Architecture Driver Version 1.0.23.
Bluetooth: Core ver 2.15
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Switching to clocksource mxc_timer1
NET: Registered protocol family 2
IP route cache hash table entries: 32768 (order: 5, 131072 bytes)
TCP established hash table entries: 131072 (order: 8, 1048576 bytes)
TCP bind hash table entries: 65536 (order: 6, 262144 bytes)
TCP: Hash tables configured (established 131072 bind 65536)
TCP reno registered
UDP hash table entries: 512 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 512 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Unpacking initramfs...
Freeing initrd memory: 176K
LPMode driver module loaded
Static Power Management for Freescale i.MX5
PM driver module loaded
sdram autogating driver module loaded
Bus freq driver module loaded
DI0 is primary
mxc_dvfs_core_probe
DVFS driver module loaded
i.MXC CPU frequency driver
DVFS PER driver module loaded
ashmem: initialized
msgmni has been set to 1805
alg: No test for stdrng (krng)
cryptodev: driver loaded.
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
regulator: get() with no identifier
By setting, SII driver will not be enabled
By setting, LDB driver will not be enabled
mxc_ipu mxc_ipu: Channel already disabled 9
mxc_ipu mxc_ipu: Channel already uninitialized 9
mxc_ipu mxc_ipu: Channel already disabled 7
mxc_ipu mxc_ipu: Channel already uninitialized 7
mxc_ipu mxc_ipu: Channel already disabled 10
mxc_ipu mxc_ipu: Channel already uninitialized 10
Serial: MXC Internal UART driver
mxcintuart.0: ttymxc0 at MMIO 0x53fbc000 (irq = 31) is a Freescale i.MX
console [ttymxc0] enabled, bootconsole disabled
console [ttymxc0] enabled, bootconsole disabled
mxcintuart.1: ttymxc1 at MMIO 0x53fc0000 (irq = 32) is a Freescale i.MX
mxcintuart.2: ttymxc2 at MMIO 0x5000c000 (irq = 33) is a Freescale i.MX
mxcintuart.3: ttymxc3 at MMIO 0x53ff0000 (irq = 13) is a Freescale i.MX
mxcintuart.4: ttymxc4 at MMIO 0x63f90000 (irq = 86) is a Freescale i.MX
loop: module loaded
pmem_adsp: 0 init
pmem_gpu: 1 init
MXC MTD nand Driver 3.0
i.MX GPMI NFC
vcan: Virtual CAN interface driver
Freescale FlexCAN Driver
FEC Ethernet Driver
fec_enet_mii_bus: probed
PPP generic driver version 2.4.2
PPP Deflate Compression module registered
PPP BSD Compression module registered
PPP MPPE Compression module registered
NET: Registered protocol family 24
tun: Universal TUN/TAP device driver, 1.6
tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.1: irq 14, io base 0x53f80200
fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
usbcore: registered new interface driver cdc_acm
cdc_acm: v0.26:USB Abstract Control Model driver for USB modems and ISDN adapter
s
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
usbcore: registered new interface driver usbserial
usbserial: USB Serial Driver core
USB Serial support registered for GSM modem (1-port)
usbcore: registered new interface driver option
option: v0.7.2:USB Driver for GSM modems
ARC USBOTG Device Controller driver (1 August 2005)
Android usb driver initialize
android_usb gadget: android_usb ready
fsl-usb2-udc: bind to driver android_usb
android gadget: register function adb
android gadget: register function usb_mass_storage
android gadget: register function rndis
rndis_function_bind_config MAC: 00:00:00:00:00:00
android_usb gadget: using random self ethernet address
android_usb gadget: using random host ethernet address
usb0: MAC 8e:92:b9:97:32:15
usb0: HOST MAC 86:e8:9e:f1:5e:36
android_usb gadget: usb_mass_storage, version: 2009/09/11
android_usb gadget: Number of LUNs=3
 lun0: LUN: removable file: (no medium)
 lun1: LUN: removable file: (no medium)
 lun2: LUN: removable file: (no medium)
mice: could not register psaux device, error: -16
mice: PS/2 mouse device common for all mice
input: gpio-keys as /devices/platform/gpio-keys/input/input0
MXC keypad loaded
egalax_ts 2-0004: request gpio failed:-16
egalax_ts 2-0004: egalax_ts: failed to read firmware version
egalax_ts: probe of 2-0004 failed with error -5
usb wakeup is here
Unknown wakeup.(OTGSC 0x8203020)
p1003_fwv33 2-0041: couldn't read panel infomation.
p1003_fwv33: probe of 2-0041 failed with error -5
DA9052 TSI Device Driver, v1.0
input: da9052_tsi as /devices/virtual/input/input1
TSI Drv Successfully Inserted da9052_tsi
input: da9052-onkey as /devices/platform/imx-i2c.0/i2c-0/0-0048/da9052-onkey/inp
ut/input2
using rtc device, mxc_rtc, for alarms
mxc_rtc mxc_rtc.0: rtc core: registered mxc_rtc as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
Linux video capture interface: v2.00
mxc_v4l2_output mxc_v4l2_output.0: Registered device video1
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v0.1.0)
APM Battery Driver
check mma8450 chip ID
mma8450 0-001c: build time Jan  3 2012 09:26:06
input: mma8450 as /devices/virtual/input/input3
add mma8450 i2c driver
MXC WatchDog Driver 2.0
MXC Watchdog # 0 Timer: initial timeout 60 sec
device-mapper: ioctl: 4.17.0-ioctl (2010-03-05) initialised: dm-devel@redhat.com

Bluetooth: Virtual HCI driver ver 1.3
Bluetooth: HCI UART driver ver 2.2
Bluetooth: HCIATH3K protocol initialized
Bluetooth: Generic Bluetooth USB driver ver 0.6
usbcore: registered new interface driver btusb
VPU initialized
mxc_asrc registered
gpu mmu enabled
mxsdhci: MXC Secure Digital Host Controller Interface driver
mxsdhci: MXC SDHCI Controller Driver.
mmc0: SDHCI detect irq 0 irq 1 INTERNAL DMA
mxsdhci: MXC SDHCI Controller Driver.
mmc1: SDHCI detect irq 203 irq 3 INTERNAL DMA
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
logger: created 64K log 'log_main'
logger: created 256K log 'log_events'
logger: created 64K log 'log_radio'
logger: created 64K log 'log_system'
Cirrus Logic CS42888 ALSA SoC Codec Driver
sgtl5000-i2c 1-000a: SGTL5000 revision 17
mxc_spdif mxc_spdif.0: MXC SPDIF Audio Transmitter
No device for codec mxc spdif
No device for DAI mxc spdif
No device for DAI imx-ssi-1-0
No device for DAI imx-ssi-1-1
No device for DAI imx-ssi-2-0
No device for DAI imx-ssi-2-1
No device for DAI imx-spdif-dai
DMA Sound Buffer Allocated: Playback UseIram=1 ext_ram=0 buf->addr=f8016000 buf-
>area=e0856000 size=24576
DMA Sound Buffer Allocated: Capture  UseIram=1 ext_ram=1 buf->addr=cf408000 buf-
>area=fb02a000 size=24576
asoc: SGTL5000 <-> imx-ssi-2-0 mapping ok
mmc0: new high speed SDHC card at address e624
mmcblk0: mmc0:e624 SU16G 14.8 GiB
 mmcblk0: p1 p2 p3 < p5 p6 > p4
DMA Sound Buffer Allocated: Playback UseIram=1 ext_ram=1 buf->addr=cf460000 buf-
>area=fb030000 size=24576
asoc: mxc spdif <-> imx-spdif-dai mapping ok
ALSA device list:
  #0: imx-3stack (SGTL5000)
  #1: imx-3stack-spdif (mxc spdif)
nf_conntrack version 0.5.0 (14443 buckets, 57772 max)
IPv4 over IPv4 tunneling driver
GRE over IPv4 tunneling driver
ip_tables: (C) 2000-2006 Netfilter Core Team
TCP cubic registered
NET: Registered protocol family 10
IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
NET: Registered protocol family 15
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Bluetooth: L2CAP ver 2.14
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO (Voice Link) ver 0.6
Bluetooth: SCO socket layer initialized
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
L2TP core driver, V2.0
PPPoL2TP kernel driver, V2.0
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 2
regulator_init_complete: incomplete constraints, leaving DA9052_BUCK_PERI on
regulator_init_complete: incomplete constraints, leaving DA9052_BUCK_MEM on
regulator_init_complete: incomplete constraints, leaving DA9052_BUCK_PRO on
regulator_init_complete: incomplete constraints, leaving DA9052_BUCK_CORE on
regulator_init_complete: incomplete constraints, leaving DA9052_LDO10 on
regulator_init_complete: incomplete constraints, leaving DA9052_LDO8 on
regulator_init_complete: incomplete constraints, leaving DA9052_LDO6 on
regulator_init_complete: incomplete constraints, leaving DA9052_LDO5 on
regulator_init_complete: incomplete constraints, leaving DA9052_LDO4 on
regulator_init_complete: incomplete constraints, leaving DA9052_LDO3 on
regulator_init_complete: incomplete constraints, leaving DA9052_LDO2 on
regulator_init_complete: incomplete constraints, leaving DA9052_LDO1 on
mxc_rtc mxc_rtc.0: setting system clock to 1970-01-13 02:29:53 UTC (1045793)
Freeing init memory: 196K
init: cannot open '/initlogo.rle'
EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
EXT4-fs (mmcblk0p5): recovery complete
EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: nodelalloc

EXT4-fs (mmcblk0p6): recovery complete
EXT4-fs (mmcblk0p6): mounted filesystem with ordered data mode. Opts: (null)

标记 (1)
0 项奖励
回复
3 回复数

1,565 次查看
HenryChiang
Contributor I

Hi Lieven

I tried your way.

It still not work.

It still hang at

~~~~~~~~~~~~~~~~~~~~~~

EXT4-fs (mmcblk0p6): recovery complete
EXT4-fs (mmcblk0p6): mounted filesystem with ordered data mode. Opts: (null)

I also change the file system from EXT4 to EXT3.

It still doesn't work and it will show EXT4.

Thanks

Lieven said:

I also had this problem with my ltib linux build. I just reformatted my flashdisk and re-copied the u-boot the kernel image and my rootsystem on ext3, afterwards it worked.

0 项奖励
回复

1,565 次查看
HenryChiang
Contributor I

HI Lieven

Thanks for help.

But I use Adeneo's demo package to setup, I will try your suggestion.

Thanks

Lieven said:

I also had this problem with my ltib linux build. I just reformatted my flashdisk and re-copied the u-boot the kernel image and my rootsystem on ext3, afterwards it worked.

0 项奖励
回复

1,565 次查看
Lyven
Contributor II

I also had this problem with my ltib linux build. I just reformatted my flashdisk and re-copied the u-boot the kernel image and my rootsystem on ext3, afterwards it worked.

0 项奖励
回复