Can't Program Flash for i.MX RT1180 EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can't Program Flash for i.MX RT1180 EVK

跳至解决方案
2,078 次查看
jett
Contributor II

I can debug through LinkServer or JLink just fine but when I try to Program Flash it fails. I have attached the Console output for the LinkServer. I am trying to flash and boot from FlexSPI qspi. Any help on this would be great thanks. 

标签 (1)
0 项奖励
回复
1 解答
2,052 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @jett ,

 

The project you want to program into the flash is a RAM target indeed, as it is for M7 which is not the default boot core of RT1180.

Kan_Li_0-1747273395216.png

 

Please use the project for M33 instead.

Kan_Li_1-1747273496211.png

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,053 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @jett ,

 

The project you want to program into the flash is a RAM target indeed, as it is for M7 which is not the default boot core of RT1180.

Kan_Li_0-1747273395216.png

 

Please use the project for M33 instead.

Kan_Li_1-1747273496211.png

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励
回复
2,028 次查看
jett
Contributor II
Thank you and I also didn't see AN14589 cleared up my remaining boot questions
0 项奖励
回复