Can't Compile SCFW Debug Monitor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't Compile SCFW Debug Monitor

ソリューションへジャンプ
2,633件の閲覧回数
philippe_schenk
Contributor IV

Hello,

 

I tried to compile SCFW with debug monitor enabled. This works fine if I do it for the MEK board:
$ make clean; make SOC=MX8QX B=mek R=b0 M=1 qx
Compiling platform/drivers/pmic/fsl_pmic.c
Compiling platform/drivers/pmic/pf8100/fsl_pf8100.c
Compiling platform/drivers/pmic/pf100/fsl_pf100.c
Compiling platform/board/mx8qx_mek/board.c
Compiling platform/board/board_common.c
Assembling platform/board/board.S
Compiling platform/board/pmic.c
Linking build_mx8qx_b0/scfw_tcm.elf ....
Objcopy build_mx8qx_b0/scfw_tcm.bin ....
done.‍‍‍‍‍‍‍‍‍‍‍


I cannot reproduce this for our board:

$ make clean; make SOC=MX8QX B=apalis R=b0 M=1 qx
Compiling platform/drivers/pmic/fsl_pmic.c
Compiling platform/drivers/pmic/pf8100/fsl_pf8100.c
Compiling platform/board/mx8qx_apalis/board.c
Compiling platform/board/board_common.c
Assembling platform/board/board.S
Linking build_mx8qx_b0/scfw_tcm.elf ....
/opt/toolchains/gcc-arm-none-eabi-8-2019-q3-update/bin/../lib/gcc/arm-none-eabi/8.3.1/../../../../arm-none-eabi/bin/ld: build_mx8qx_b0/main/monitor.o: in function `cmd_pmic':
/home/bamboo/automation/sumo-4.14.98-2.3.0/bsp_pkg_mx8/temp_build_dir/build-imx8qmmek/tmp/work/imx8qmmek-poky-linux/imx-scfw-porting-kit/1.3.1+gitAUTOINC+b929edfe9e-r0/git/firmware/platform/main/monitor.c:2554: undefined reference to `dynamic_pmic_register_access'
/opt/toolchains/gcc-arm-none-eabi-8-2019-q3-update/bin/../lib/gcc/arm-none-eabi/8.3.1/../../../../arm-none-eabi/bin/ld: /home/bamboo/automation/sumo-4.14.98-2.3.0/bsp_pkg_mx8/temp_build_dir/build-imx8qmmek/tmp/work/imx8qmmek-poky-linux/imx-scfw-porting-kit/1.3.1+gitAUTOINC+b929edfe9e-r0/git/firmware/platform/main/monitor.c:2578: undefined reference to `dynamic_pmic_register_access'
/opt/toolchains/gcc-arm-none-eabi-8-2019-q3-update/bin/../lib/gcc/arm-none-eabi/8.3.1/../../../../arm-none-eabi/bin/ld: build_mx8qx_b0/main/monitor.o: in function `cmd_pmic_list_8100':
/home/bamboo/automation/sumo-4.14.98-2.3.0/bsp_pkg_mx8/temp_build_dir/build-imx8qmmek/tmp/work/imx8qmmek-poky-linux/imx-scfw-porting-kit/1.3.1+gitAUTOINC+b929edfe9e-r0/git/firmware/platform/main/monitor.c:2640: undefined reference to `dynamic_pmic_get_voltage'
/opt/toolchains/gcc-arm-none-eabi-8-2019-q3-update/bin/../lib/gcc/arm-none-eabi/8.3.1/../../../../arm-none-eabi/bin/ld: /home/bamboo/automation/sumo-4.14.98-2.3.0/bsp_pkg_mx8/temp_build_dir/build-imx8qmmek/tmp/work/imx8qmmek-poky-linux/imx-scfw-porting-kit/1.3.1+gitAUTOINC+b929edfe9e-r0/git/firmware/platform/main/monitor.c:2649: undefined reference to `dynamic_pmic_get_voltage'
collect2: error: ld returned 1 exit status
make: *** [Makefile:555: build_mx8qx_b0/scfw_tcm.elf] Error 1‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍


I compared the MEK board file and ours, but can't spot any difference regarding this linker errors. Could you please help me getting that compiled and the bug fixed so we are able to use the debug monitor too in the future?

 

Thanks and Best Regards
Philippe

 

FYI: Raluca Popa

1 解決策
2,543件の閲覧回数
philippe_schenk
Contributor IV

We were able to solve the issue ourselves, it was a missing thing in Makefile that we didn't port over:

diff --git a/src/scfw_export_mx8qx_b0/platform/board/mx8qx_apalis/Makefile b/src/scfw_export_mx8qx_b0/platform/board/mx8qx_apalis/Makefile
index 0f8901e..b04746f 100644
--- a/src/scfw_export_mx8qx_b0/platform/board/mx8qx_apalis/Makefile
+++ b/src/scfw_export_mx8qx_b0/platform/board/mx8qx_apalis/Makefile
@@ -48,3 +48,6 @@ CTRL_MD += $(SRC)/board/mx8qx_$(B)/control.txt
DIRS += $(OUT)/board/mx8qx_$(B)
+ifeq ($(M),1)
+ OBJS += $(OUT)/board/pmic.o
+endif
diff --git a/src/scfw_export_mx8qx_b0/platform/board/mx8qx_apalis/board.bom b/src/scfw_export_mx8qx_b0/platform/board/mx8qx_apalis/board.bom
index f129642..68d9ada 100755
--- a/src/scfw_export_mx8qx_b0/platform/board/mx8qx_apalis/board.bom
+++ b/src/scfw_export_mx8qx_b0/platform/board/mx8qx_apalis/board.bom
@@ -34,3 +34,6 @@ DRV2 += \
pmic \
pmic/pf8100
+ifeq ($(M),1)
+ DRV2 += pmic/pf100
+endif‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,544件の閲覧回数
philippe_schenk
Contributor IV

We were able to solve the issue ourselves, it was a missing thing in Makefile that we didn't port over:

diff --git a/src/scfw_export_mx8qx_b0/platform/board/mx8qx_apalis/Makefile b/src/scfw_export_mx8qx_b0/platform/board/mx8qx_apalis/Makefile
index 0f8901e..b04746f 100644
--- a/src/scfw_export_mx8qx_b0/platform/board/mx8qx_apalis/Makefile
+++ b/src/scfw_export_mx8qx_b0/platform/board/mx8qx_apalis/Makefile
@@ -48,3 +48,6 @@ CTRL_MD += $(SRC)/board/mx8qx_$(B)/control.txt
DIRS += $(OUT)/board/mx8qx_$(B)
+ifeq ($(M),1)
+ OBJS += $(OUT)/board/pmic.o
+endif
diff --git a/src/scfw_export_mx8qx_b0/platform/board/mx8qx_apalis/board.bom b/src/scfw_export_mx8qx_b0/platform/board/mx8qx_apalis/board.bom
index f129642..68d9ada 100755
--- a/src/scfw_export_mx8qx_b0/platform/board/mx8qx_apalis/board.bom
+++ b/src/scfw_export_mx8qx_b0/platform/board/mx8qx_apalis/board.bom
@@ -34,3 +34,6 @@ DRV2 += \
pmic \
pmic/pf8100
+ifeq ($(M),1)
+ DRV2 += pmic/pf100
+endif‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍
0 件の賞賛
返信