Can someone provide documentation for using the RPMsg-Lite with Android configuration for imx8mn?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can someone provide documentation for using the RPMsg-Lite with Android configuration for imx8mn?

1,866 Views
anurag16doshi
Contributor III

I am working with the iMX8 Nano Evaluation Board. I have downloaded the MCUExpresso SDK for testing out certain applications for the M7 core. I want to use the RPMsg-Lite for communication between the A53 and M7. As per my understanding the applications provided in the SDK are for Linux Configurations. I am looking to have the A53 core running Android and not Linux.

1. Is there documentation available for the RPMsg-Lite to be used for an Android configuration? If yes, can someone provide me the links for the same?

2. If possible can the SDK code be converted for a Android configuration from a for Linux configuration?

TIA,

Anurag

0 Kudos
Reply
1 Reply

1,843 Views
b36401
NXP Employee
NXP Employee

We have no such examples for Android. Sorry for the inconvenience.
We only suggest you to refer the documents like this as a reference:
https://community.nxp.com/docs/DOC-343113

0 Kudos
Reply