Can not connect to git.freescale.com when trying to build yocto krogoth

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can not connect to git.freescale.com when trying to build yocto krogoth

2,336 次查看
xiongqr
Contributor I

WARNING: firmware-imx-1_5.4-r0 do_fetch: Failed to fetch URL git://git.freescale.com/imx/imx-firmware.git;branch=master;destsuffix=/home/jenkins/tnAp6212/technexion/technexion.1/local_build/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/firmware-imx/1_5.4-r0/firmware-imx-5.4/git, attempting MIRRORS if available
ERROR: firmware-imx-1_5.4-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 128, output:
Cloning into bare repository '/opt/dl_dir.tn_ap6212/git2/git.freescale.com.imx.imx-firmware.git'...
fatal: unable to connect to git.freescale.com:
git.freescale.com[0: 192.88.156.202]: errno=Connection refused


ERROR: firmware-imx-1_5.4-r0 do_fetch: Function failed: Fetcher failure for URL: 'git://git.freescale.com/imx/imx-firmware.git;branch=master;destsuffix=/home/jenkins/tnAp6212/technexion/technexion.1/local_build/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/firmware-imx/1_5.4-r0/firmware-imx-5.4/git'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/jenkins/tnAp6212/technexion/technexion.1/local_build/tmp/work/cortexa9hf-neon-mx6qdl-poky-linux-gnueabi/firmware-imx/1_5.4-r0/temp/log.do_fetch.31097
ERROR: Task 2720 (/home/jenkins/tnAp6212/technexion/technexion.1/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/firmware-imx/firmware-imx_5.4.bb, do_fetch) failed with exit code '1'

标签 (1)
1 回复

1,792 次查看
joanxie
NXP TechSupport
NXP TechSupport

the source code was moved to "https://source.codeaurora.org/external/imx", try to change the ""git://git.freescale.com/imx" " to "https://source.codeaurora.org/external/imx"