Can not close window

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
7,136件の閲覧回数
ko-hey
Senior Contributor II

Hi all

I'm using MCIMX6DL-SDP with Yocto Linux that provided from freescale.

In that situation, I can not close the window from touch pannel.

However, if I use a mouse that connect with USB, I can close it. (The button is like a attachment.)

sample.jpg

I tried to re-calibration and reset but behavior does not change.

I can not understand the cause.


Please advise me!



Best Regards,

ラベル(3)
0 件の賞賛
返信
1 解決策
6,759件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
13 返答(返信)
6,760件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
6,759件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

using evtest (i.e.) can you see if you can actually "click" over the X button?

It may be 2 problems:

calibration not working

exit not working

0 件の賞賛
返信
6,759件の閲覧回数
ko-hey
Senior Contributor II

Hi Daiane & Yixing

Thank you for your response.

I checked a problem with using Terminal app that is in Yocto project.

The command is below.

$ evtest /dev/input/touchscreen

When I touched X button, some value are shown in terminal app. So I think touchscreen is work.

After that I retried a calibration with Calibration app. However, nothing was changed.

Finally, I checked a USB mouse behavior with a command as below.

It is no problem with a behavior of the USB mouse.

$ cat /dev/input/mice

Best Regards,

ko-hey

0 件の賞賛
返信
6,759件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

When you touch over the X (the X closer button), can the evtest return the right (x,y) values?

Or the (x,y) values are outside the X button?

And, additionally, take a look here http://git.yoctoproject.org/cgit/cgit.cgi/meta-fsl-arm/tree/recipes-graphics/xinput-calibrator

on how to configure the calibration for your HW and your display

0 件の賞賛
返信
6,759件の閲覧回数
ko-hey
Senior Contributor II

What is a correct value?

Some values are shown in display, when I touched the screen.

But I don't know whether the value is correct.

And I have a question about configuration method.

Can I use these commands to configure the calibration ?

xinput set-int-prop "eGalax Touch Screen" "Evdev Axis Calibration" 42060 2062 -8 -783544 1 1549 65536

xinput set-int-prop "eGalax Touch Screen" "Evdev Axes Swap" 8 0

0 件の賞賛
返信
6,759件の閲覧回数
YixingKong
Senior Contributor IV

Ko-Hey, if your issue is gone, please close the DI, otherwise please keep working with the engineers.

Thanks,

Yixing

0 件の賞賛
返信
6,759件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

the problem is exactly to find the right number to place in the conf file.

each panel has its own right number. you must to play around with your

0 件の賞賛
返信
6,759件の閲覧回数
ko-hey
Senior Contributor II

Hi Daiane

Sorry for my late reply. I was on vacation until yesterday.

I understood each panel has its own value.

Which conf file do I check for find a correct value?

Addition to this, please let me know how to set a correct value.

I have a additional info.

When I touched a X button, below value was returned.

-------------- Report sync ------------

type 3 (Absolute), code 57 (Tracking ID), value 0

type 3 (Absolute), code 48 (Touch Major), value 1

type 3 (Absolute), code 53 (Position X), value 32176

type 3 (Absolute), code 54 (Position Y), value 288

-------------- Config sync ------------

Ko-hey

0 件の賞賛
返信
6,759件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

I have no idea ko-hey, I used the trial and error method.

0 件の賞賛
返信
6,759件の閲覧回数
ko-hey
Senior Contributor II

Do you said that you don't know the location of the file?

If yes, please check to expert engineers.

If you tell me the file location, I will check the file too.

Also I would like to check your situation.

Was this problem occurred on your board?

0 件の賞賛
返信
6,759件の閲覧回数
YixingKong
Senior Contributor IV

Ko-Hey

There is no action for this isue for long time. If there is no issue, we will close this DI. If you still need help please kep commenting here.

Thanks,

Yixing

0 件の賞賛
返信
6,759件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

I´m sorry, I was unclear.

The file you should edit is the one I have already linked in this thread.

the *value* to put into the file is up to you to find out because it depends on your hardware piece.

Let me try to explain it again.

You hardware must be calibrated, because each hardware is unique.

You calibrate it using the calibration app.

But sometimes the base values is so far from real that even the calibration app can actually calibrate your panel. So you need to add *by hand* some guessing numbers. The example for this is in the link I have already sent to you.

However, I don't know if your problem is the calibration, because the very first question you made is regarding not closing the windows. I guessed it *may* be the calibration, but I cannot be sure.

Kernel is not, because you have already tested evtest and kernel is returning events.

So, if this is a calibration error, maybe you can get better help from the calibration app community

If this is really a QT error (are you using QT?) maybe you should contact QT community.

You asked for advises, I tried to help the in my best way. I'm sorry if this was not enough. The way I made the file I sent you the link, worked for me. It was a long time ago (2013-03-30) how you can see in meta-fsl-arm - Layer containing Freescale ARM hardware support metadata

0 件の賞賛
返信
6,759件の閲覧回数
YixingKong
Senior Contributor IV

The request has been assigned.

Thanks,

Yixing

0 件の賞賛
返信