Can not Boot from SD Card with Linux and i.MX6 SABRE SD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not Boot from SD Card with Linux and i.MX6 SABRE SD

Jump to solution
4,086 Views
peteramond
Contributor V

Hi All,

#Yuri Muhin

I can not figure out why the SABRE SD board does not boot from the SD Card when I put Linux on it. Recently I bought i.mx6 quad Sabre SDB development board and I got a bootable  SD card with Android OS. When I put linux on it; it is not working.

  1. Could you please give me the link for suitable linux image for imx6 quad Sabre SDB board.
  2. Don't we have the complete linux bootable image for sabre sdb (with uboot and partitioned image) ? Is there any special way to write SD card to boot in sabre SDB development board ?
  3. Can I use this gz zip file >> http://www.freescale.com/webapp/Download?colCode=L3.14.28_1.0.0_iMX6QDLS_BUNDLE  << How can I chose correct image file for this ? Do I need to write complete gz file in SD card ?

I must be thankful to you if you will kindly reply me soon.

Regards,

Peter.

Labels (3)
1 Solution
3,027 Views
Yuri
NXP Employee
NXP Employee

Hello,

generally HDMI environment settings are described in the following thread.

HDMI Audio Setting 

  Usually problems relate to incorrect U-boot environment setting.
The line should not contain such codes as space in parameter block (say, for HDMI) or LF.

setenv mmcargs 'setenv bootargs console=${console},${baudrate} ${smp} root=/dev/mmcblk2p2
rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24'


Below is useful link :

https://community.nxp.com/message/847843?commentID=847843#comment-847843 

Regards,

Yuri.

View solution in original post

5 Replies
3,027 Views
Yuri
NXP Employee
NXP Employee

Hello,

   

Please try to prepare boot SD card, using NXP demo image, and boot it.
It is the simplest way to check boot options on the SDB.

The SD card demo image (it has .sdcard file extension) may be found on the NXP Web.

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_MX6QDLSOLO&appType=license&location=null&Pa... 

Summary Page :

i.MX 6 Series Software and Development Tool|NXP 

You may apply Win32DiskImager to copy the image to SD card under Windows host.

< https://sourceforge.net/projects/win32diskimager/ >

Regards,

Yuri.

3,028 Views
peteramond
Contributor V

Hi Yuri,

Many thanks for your quick response. 

I did every thing according to your instructions and burned the SD card with " fsl-image-validation-imx-x11-imx6qdlsolo.sdcard " image and now the Sabre SDB board boot correctly. Thanks for your instructions.

But again I have a problem with HDMI output and it shows that " HDMI video is not ready ! "

pastedImage_1.png

Could you please advice on this ? I tried with " fsl-image-qt5-validation-imx-x11-imx6qdlsolo.sdcard " image also and but there is no any change.

Regards,

Peter.

0 Kudos
Reply
2,105 Views
B_Prabhu
Contributor III

Hi,

Can you help me how do you done the flashing? Can you explain me in detail?

I have same board what you purchased but i couldn't able to boot up the board.

0 Kudos
Reply
3,028 Views
Yuri
NXP Employee
NXP Employee

Hello,

generally HDMI environment settings are described in the following thread.

HDMI Audio Setting 

  Usually problems relate to incorrect U-boot environment setting.
The line should not contain such codes as space in parameter block (say, for HDMI) or LF.

setenv mmcargs 'setenv bootargs console=${console},${baudrate} ${smp} root=/dev/mmcblk2p2
rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24'


Below is useful link :

https://community.nxp.com/message/847843?commentID=847843#comment-847843 

Regards,

Yuri.

3,028 Views
bernhardfink
NXP Employee
NXP Employee

There is always a chance that specific SD cards don't work for booting Linux. I have multiple cards from different manufacturers which look fine on the PC, but don't boot. However, same cards with Android might work fine.

So if you can't make above mentioned sdcard image working, simply try it with other SD cards.

Regards,

Bernhard.