Can imx6dual encode continuous RGB bitmaps to H264 video stream?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can imx6dual encode continuous RGB bitmaps to H264 video stream?

1,150 Views
zoushx
Contributor I

Can imx6dual encode continuous RGB bitmaps to H264 video stream? The RGB bitmaps is received from eithernet ,15 frames per second,320*256 pixels,and the H264 video stream is send out through wifi.This is to say,the imx6dual is used to encode BMPs to H264 video.Can imx6dual do this? If can,how to realize?Please give me some adivce.

Labels (3)
0 Kudos
Reply
1 Reply

1,104 Views
igorpadykov
NXP Employee
NXP Employee

Hi zou

for supported formats please refer to sect.3.2.2 Data and Structure Definitions

attached VPU Linux Guide. In general one can try to use CSC with examples described on

https://community.freescale.com/docs/DOC-94961

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply