Can i use the Mfgtool from commandline

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can i use the Mfgtool from commandline

ソリューションへジャンプ
2,646件の閲覧回数
anch
Contributor I

Can i use the Mfgtool from commandline. I can flash my iMX6 from UI.

To use Mfgtool from commandline, i have used this command "MfgTool2.exe –noui –c “MX6Q Linux Update” –l “Sabre-SD” –p 4"

but the problem is it opens the Userinterface. It doesnot flash when i close the UI. Does anyone has any idea?

0 件の賞賛
返信
1 解決策
4 返答(返信)
2,133件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please use the recent MFG, where scripts .vbs in the MFG package may be used.

Set wshShell = CreateObject("WScript.shell")

  1. wshShell.run "mfgtool2.exe -noui -c ""linux"" -l ""SDCard"" -s ""board=sabresd"" -s ""mmc=0"" "

Set wshShell = Nothing


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,133件の閲覧回数
anch
Contributor I

hi Yuri

thanks for the response, this post definitely answers my question. but could you tell me where i could find the latest MFG.

When i did a search, i found only the source code, which says it can be used for imX50, 51... but not iMX6.

Do i have to build the source code or i can i download it somewhere on the site?

I have found one Mfgtool for downloading images to iMX6 series, Rev 12.10.02. Can i use this from command line?

Thanks

0 件の賞賛
返信
2,133件の閲覧回数
anch
Contributor I

thanks for the links Yuri.

I will give it a try.

thanks once agaubn

0 件の賞賛
返信