Can i have example source for EMIF(External memory interface) function?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can i have example source for EMIF(External memory interface) function?

2,566件の閲覧回数
hanseunglee
Contributor III

I check i.mx6dl interface for data transfer from fpga chip.

so.. if i.mx6 sabresd board can use EMIF function, can i have example code or manual?

I already search unit_test example folder but i can not find EMIF file.

If you know every information about EMIF, reply please.

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

2,300件の閲覧回数
ruiguo
Contributor II

Hi Hanseung

I am glad to read your article for EIM and FPGA.I am studying them in our work. But I meet a hard problem that the signal is not produced in the EIM bus. I hope you can help me to share your code. sincerely! I look forward to your replay.

Rui

0 件の賞賛
返信

2,300件の閲覧回数
art
NXP Employee
NXP Employee

The i.MX6DualLite processor has many various interfaces to receive data from FPGA. Those are the parallel External Memory Interface Module (EIM, primarily meant for connection of an external SRAM/NOR Flash like memories), parallel Camera Sensor Interface (CSI) that allows raw data transfer to memory, PCIe (if supported by FPGA). The particular connection method is FPGA-dependent.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信