Can i.MX8MM run in lower frequency ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i.MX8MM run in lower frequency ?

1,222 Views
jimmyli
Contributor IV

Hi,

      I have a question that can i.mx8mm runing in 800MHz@A53 core ?

      Sometimes, we need to run lower frequency of A53 core to decrease power consumption.

      Thanks very much.

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,174 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @jimmyli,

I hope you are doing well.

One needs to add opp table points in imx8mm.dtsi for lower frequency support.

Please refer to a53_opp_table node in /arch/arm64/boot/dts/freescale/imx8mm.dtsi

One can refer to the patch mentioned in https://community.nxp.com/t5/i-MX-Processors/Lower-CPU-frequency-on-imx8mm/td-p/955456

Please also add the PLL rate for lower frequency in /drivers/clk/imx/clk-pll14xx.c

I hope it helps!

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply

1,164 Views
jimmyli
Contributor IV

Hi Ritech,

         Thanks for your replying.

         I will try again.

0 Kudos
Reply