Can cortexm4 be used for general purpose in imx8, imx8x?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can cortexm4 be used for general purpose in imx8, imx8x?

ソリューションへジャンプ
1,229件の閲覧回数
yibhan
Contributor III

Dear NXP,

While running a Linux application with imx8x, I want to control real-time motors separately with cortex M4. I want to control the motor in real time using cortexM4 alone. Is this possible? If not, I would like to recommend a soc among the imx processors that would satisfy my needs. If it is not possible with a single processor, I am curious as to whether a combination of nxp chips is possible. We are planning a product that controls motor control in real time while processing camera images and images in the main program.
When using MCU in motor control, there are communication speed limitations with the imx processor and communication processing delays, so we want to secure real-time through data sharing using a shared memory method using cortexM4 within the same soc.
I would like to use OpenAMP (Open Asymemtric Multi-Processing), but would you like guidance on whether it is possible on an imx processor based on Linux?

I look forward to your helpful response.

 

 

0 件の賞賛
返信
1 解決策
1,127件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @yibhan 

 

You can have access to the LSIO Subsystem and configure it with the RDC. Please refer to the Cortex M SDK examples. Then you will be able to control the LSIO:

Alejandro_Salas_0-1725906319148.png

 

Best regards,

Salas.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,208件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @yibhan 

I hope you are doing well.

Yes, the i.MX8 processors have a combination of Cortex A and Cortex M cores, that you can use the Cortex A to handle an operating system as Linux, Android, etc. And the Cortex M can handle real time applications. NXP provide the SDK for the Cortex M cores.

For communication between cores, i.MX8 processors support RPMSG, you can find the information on the i.MX Linux Reference Manual, please refer to the chapter 2.8 Remote Processor Messaging.

 

I hope this information can helps to you.

 

Best regards,

Salas.

0 件の賞賛
返信
1,202件の閲覧回数
yibhan
Contributor III

Dear NXP,

Thank you for your response, but I have additional questions.

As shown in the block diagram below, there is a User CortexM4 complex, with one available UART/I2C/GPIO allocated to each. However, in my case, if you want to control a motor, you need PWM (4), GPIOs (10), and UART (1), which are lacking in the User CM4 complex. How to solve this?

yibhan_1-1725406310917.png

 

0 件の賞賛
返信
1,128件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @yibhan 

 

You can have access to the LSIO Subsystem and configure it with the RDC. Please refer to the Cortex M SDK examples. Then you will be able to control the LSIO:

Alejandro_Salas_0-1725906319148.png

 

Best regards,

Salas.

0 件の賞賛
返信
1,096件の閲覧回数
yibhan
Contributor III
Thank you for answering