Can bus function on i.MX6q with Android 5.0.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can bus function on i.MX6q with Android 5.0.2

2,214 次查看
jim2_chen
Contributor I

I have modify kernel to enable flexcan on SabreSD board and I can find can0 when system boot up.

But when I try to bring up can0 with "ip link set can0 up type can bitrate 125000" I find two IRQ error from kernel message:

flexcan 2090000.can can0: writing ctrl=0x0e312005

flexcan 2090000.can can0: flexcan_set_bittiming: mcr=0x5980000f ctrl=0x0e312005

flexcan 2090000.can can0: flexcan_chip_start: writing mcr=0x7de2020d

flexcan 2090000.can can0: flexcan_chip_start: writing ctrl=0x0e31ac55

flexcan 2090000.can can0: flexcan_chip_start: reading mcr=0x6de2020d ctrl=0x0e31ac55

flexcan 2090000.can can0: Error Warning IRQ

flexcan 2090000.can can0: Error Passive IRQ

flexcan 2090000.can can0: bus-off

When I try to send packet from can0 by cansend, I can't measure any change from TX pin.

Does anyone know the problem of it?

标签 (4)
2 回复数

1,670 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jim

by default SabreSD BSP does not support flexcan, please follow

guidelines on

How to enable CAN bus on i.MX6Q SabreSD

How to use FlexCAN in Android OS

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,670 次查看
jim2_chen
Contributor I

Hi igorpadykov ,

Thanks for your reply. But unfortunately, these information are not useful for my condition. These environments are not the same as Android 5.0.2 released by NXP. My problem is the bus will become bus-off when I bring it up. I have trace flexcan.c in drivers/net/can/ and I guess the bus-off is come from flexcan_poll_state() and in do_state() it will call can_bus_off if new_state is CAN_STATE_BUS_OFF. I can't find any discuss about this issue on community. How can I prevent the can bus become bus-off?

0 项奖励
回复