Can anybody download LF_v6.1.55-2.2.0_images_IMX93EVK images?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can anybody download LF_v6.1.55-2.2.0_images_IMX93EVK images?

Jump to solution
2,743 Views
gyyang
Contributor I

Hello,

I'm trying to download latest image of I.mx93 (LF_v6.1.55-2.2.0_images_IMX93EVK) to the EVK via USB serial downlaod.

But everytime I tried, I got below message. [HID(W):LIBUSB_ERROR_PIPE ]

====================

uuu -b emmc_all imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot imx-image-multimedia-imx93-11x11-lpddr4x-evk.wic.zst


uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.141-0-gde317f5

Success 0 Failure 1

2:3 1/ 1 [HID(W):LIBUSB_ERROR_PIPE ] SDPS: boot -scanterm -f imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-f

I also tried latest pre-release version of uuu( 1.5.141) which says, Hot Fixed for SPDS crash for some images, but without success.

==============

Can I just use "uuu uuu.auto-imx93evk" for downloading?

Thanks!

 

0 Kudos
Reply
1 Solution
2,475 Views
joanxie
NXP TechSupport
NXP TechSupport

as I known, the new bsp only support A1, I suggest that you can contact local DFAE to check if they can offer A1 board or not

https://www.nxp.com/support/sample-and-buy/distributor-network:DISTRIBUTORS

View solution in original post

0 Kudos
Reply
15 Replies
2,731 Views
joanxie
NXP TechSupport
NXP TechSupport

I haven't download this version image yet, I will test for you later, but how about using the command like

uuu -b emmc_all imx-image-multimedia-imx93-11x11-lpddr4x-evk.wic.zst

since from version 4.14.165, you can download wic or zst images directly

joanxie_0-1703234672027.png

by the way, I download this prebuilt image package, I don't find imx-image-multimedia-imx93-11x11-lpddr4x-evk.wic.zst there, only imx-image-multimedia-imx93-evk.wic, where did you get imx-image-multimedia-imx93-11x11-lpddr4x-evk.wic.zst?

0 Kudos
Reply
2,706 Views
gyyang
Contributor I

Thank you for the reply, joanxie

I tried "uuu -b emmc_all imx-image-multimedia-imx93evk.wic" but failed with same code.

And sorry for the file name, I mixed up the file name with the filename that I had built.

I tried to download both images pre-built and my own. Result is same everytime.

Again Thanks.

0 Kudos
Reply
2,698 Views
joanxie
NXP TechSupport
NXP TechSupport

I downloaded 6.1.55 demo images, download to the board without issue, this is steps:

1) use the USB1 as download usb port

2) set he SW1301 as 1100[1-4]

3) the command is below

joanxie_1-1703584349631.png

 

 

 

 

0 Kudos
Reply
2,677 Views
gyyang
Contributor I

Thank you joanxie,

I'm doing exactly the same but fails always. Could you please let me know the version of uuu.

I'm afraid this could be a driver issue.

Regards,

0 Kudos
Reply
2,668 Views
joanxie
NXP TechSupport
NXP TechSupport

I already attached the uuu version I used, which is 1.5.21

0 Kudos
Reply
2,671 Views
joanxie
NXP TechSupport
NXP TechSupport

do you use A1 board? refer to the release note, this bsp only supports i.MX 93 EVK board (11x11 A1 silicon), if you use A0 board, you couldn't use this version

0 Kudos
Reply
2,664 Views
gyyang
Contributor I
Thank you for the quick reply.
I'm not sure what is the version of my EVK. Where can I find the board version?
0 Kudos
Reply
2,662 Views
joanxie
NXP TechSupport
NXP TechSupport

pls give me back of  your board picture

0 Kudos
Reply
2,654 Views
gyyang
Contributor I

Thanks,

Here is the picture of my board.

Regards,

 

0 Kudos
Reply
2,644 Views
joanxie
NXP TechSupport
NXP TechSupport

I need the picture for back of board

0 Kudos
Reply
2,592 Views
gyyang
Contributor I

Sorry,

Here is the back of the board.

Thanks.

0 Kudos
Reply
2,560 Views
joanxie
NXP TechSupport
NXP TechSupport

it seems this is A0 board, try to test Linux 6.1.22_2.0.0​ again

https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for...

0 Kudos
Reply
2,479 Views
gyyang
Contributor I

Thank you joanxie,

I could download images from 6.1.22_2. Definitely, my board has A0 silicon. Thank you again.

Do you have any information about plans on Linux release that support i.mx93 A0 scilicon? I need to use Audio HAT with i.mx93 board, but it seams 6.1.22_2 release does not support Audio HAT yet.

regards,

 

0 Kudos
Reply
1,922 Views
nxp29347
NXP Employee
NXP Employee

Hi, so I tried both:

LF_v6.1.55-2.2.0_images_IMX93EVK

and

LF_v6.1.22-2.0.0_images_IMX93EVK

but both times I get

2:4 1/ 1 [HID(W):LIBUSB_ERROR_PIPE ] SDPS: boot -scanterm -f imx-image-full-imx93evk.wic -scanlimited 0x800000

My uuu is:

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.125-0-gaeb3490

On the backside of my board it says

... REV B

... REV B5

is this sufficient to know the which version it is? If not how do I find out?

I actually also tried to flash the

imx-image-full-imx93evk.wic

file to an sd card and boot from there, which also didn't work ...

What else could I try ...???

Thx

0 Kudos
Reply
2,476 Views
joanxie
NXP TechSupport
NXP TechSupport

as I known, the new bsp only support A1, I suggest that you can contact local DFAE to check if they can offer A1 board or not

https://www.nxp.com/support/sample-and-buy/distributor-network:DISTRIBUTORS

0 Kudos
Reply