[I.MX8M Plus] using DMA to do memory copy from RAM to RAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[I.MX8M Plus] using DMA to do memory copy from RAM to RAM

ソリューションへジャンプ
3,099件の閲覧回数
linzhenggang1
Contributor II

Is it possible to do a RAM-to-RAM memory copy using DMA?

If yes, how should we do that in Linux?

P.S. We are using BSP L6.1.22

0 件の賞賛
返信
1 解決策
2,977件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, it's correct!, if you like to copy RAM to RAM can use the SDMA but The current drivers don't have the API to do it.

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,074件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes it is possible, but you need to clarify which memory to what memory are you using, you can use the provided driver in the BSP.

Regards

0 件の賞賛
返信
3,064件の閲覧回数
linzhenggang1
Contributor II

Thank you for your reply.

Sorry, I don't understand the meaning of "which RAM and what RAM" you said.
I just want to do a memory copy in a user-space application(not from or to a peripheral) by using DMA to reduce my CPU usage.

If it is possible, could you please show me which part of the BSP I should use to do that?

Thank you very much!

0 件の賞賛
返信
3,041件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

There is no code to show how to use dma, but one can show the section 3.7.3 of the linux reference manual:

https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf

 

Regards

 

0 件の賞賛
返信
2,983件の閲覧回数
linzhenggang1
Contributor II

Thank you for your reply.

In 3.7.1, it said that the SDMA API driver is for other drivers(kernel mode) but not for a user space application. Is my understanding correct?

---

3.7.1 Overview
The Smart Direct Memory Access (SDMA) API driver controls the SDMA hardware. It provides an API to other
drivers for transferring data between MCU memory space and the peripherals. It supports the following features:

0 件の賞賛
返信
2,978件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, it's correct!, if you like to copy RAM to RAM can use the SDMA but The current drivers don't have the API to do it.

Regards

0 件の賞賛
返信