Hello,
I'm trying to download latest image of I.mx93 (LF_v6.1.55-2.2.0_images_IMX93EVK) to the EVK via USB serial downlaod.
But everytime I tried, I got below message. [HID(W):LIBUSB_ERROR_PIPE ]
====================
uuu -b emmc_all imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot imx-image-multimedia-imx93-11x11-lpddr4x-evk.wic.zst
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.141-0-gde317f5
Success 0 Failure 1
2:3 1/ 1 [HID(W):LIBUSB_ERROR_PIPE ] SDPS: boot -scanterm -f imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-f
I also tried latest pre-release version of uuu( 1.5.141) which says, Hot Fixed for SPDS crash for some images, but without success.
==============
Can I just use "uuu uuu.auto-imx93evk" for downloading?
Thanks!
解決済! 解決策の投稿を見る。
as I known, the new bsp only support A1, I suggest that you can contact local DFAE to check if they can offer A1 board or not
https://www.nxp.com/support/sample-and-buy/distributor-network:DISTRIBUTORS
I haven't download this version image yet, I will test for you later, but how about using the command like
uuu -b emmc_all imx-image-multimedia-imx93-11x11-lpddr4x-evk.wic.zst
since from version 4.14.165, you can download wic or zst images directly
by the way, I download this prebuilt image package, I don't find imx-image-multimedia-imx93-11x11-lpddr4x-evk.wic.zst there, only imx-image-multimedia-imx93-evk.wic, where did you get imx-image-multimedia-imx93-11x11-lpddr4x-evk.wic.zst?
Thank you for the reply, joanxie
I tried "uuu -b emmc_all imx-image-multimedia-imx93evk.wic" but failed with same code.
And sorry for the file name, I mixed up the file name with the filename that I had built.
I tried to download both images pre-built and my own. Result is same everytime.
Again Thanks.
I downloaded 6.1.55 demo images, download to the board without issue, this is steps:
1) use the USB1 as download usb port
2) set he SW1301 as 1100[1-4]
3) the command is below
Thank you joanxie,
I'm doing exactly the same but fails always. Could you please let me know the version of uuu.
I'm afraid this could be a driver issue.
Regards,
I already attached the uuu version I used, which is 1.5.21
do you use A1 board? refer to the release note, this bsp only supports i.MX 93 EVK board (11x11 A1 silicon), if you use A0 board, you couldn't use this version
pls give me back of your board picture
I need the picture for back of board
it seems this is A0 board, try to test Linux 6.1.22_2.0.0 again
Thank you joanxie,
I could download images from 6.1.22_2. Definitely, my board has A0 silicon. Thank you again.
Do you have any information about plans on Linux release that support i.mx93 A0 scilicon? I need to use Audio HAT with i.mx93 board, but it seams 6.1.22_2 release does not support Audio HAT yet.
regards,
Hi, so I tried both:
LF_v6.1.55-2.2.0_images_IMX93EVK
and
LF_v6.1.22-2.0.0_images_IMX93EVK
but both times I get
2:4 1/ 1 [HID(W):LIBUSB_ERROR_PIPE ] SDPS: boot -scanterm -f imx-image-full-imx93evk.wic -scanlimited 0x800000
My uuu is:
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.125-0-gaeb3490
On the backside of my board it says
... REV B
... REV B5
is this sufficient to know the which version it is? If not how do I find out?
I actually also tried to flash the
imx-image-full-imx93evk.wic
file to an sd card and boot from there, which also didn't work ...
What else could I try ...???
Thx
as I known, the new bsp only support A1, I suggest that you can contact local DFAE to check if they can offer A1 board or not
https://www.nxp.com/support/sample-and-buy/distributor-network:DISTRIBUTORS