Can a HAB Encrypted Image Boot and Run from Internal Flash in i.MXRT10xx ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can a HAB Encrypted Image Boot and Run from Internal Flash in i.MXRT10xx ?

539 Views
mjpovi
Contributor III

Hi,
I wish to confirm my understanding of HAB Secure/Encrypted boot in that a HAB Encrypted image cannot be flashed or be booted and run XIP from the internal flash on an IMXRT10xx MCU.  HAB encrypted flashing/boot XIP is only supported using external flash (or executing from OCRAM) ? 

0 Kudos
Reply
1 Reply

507 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @mjpovi ,

Thanks for your interest in NXP MIMXRT series!

No. In fact, for the RT series, there is little difference between the so-called internal Flash and external Flash, both of which are connected using the FlexSPI. And HAB encrypted boot, does not support XIP.

Best regards,
Gavin

0 Kudos
Reply