Can UART3 in the iMX6 SDK function as Debug Uart ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can UART3 in the iMX6 SDK function as Debug Uart ?

2,234件の閲覧回数
os
Contributor I

I have a board similar to the iMX6Q Sabre SDB. I have the debug serial port connected to UART3 (pins EIM_D24/25). I am running the "Platform SDK (1.1) for MX6DQ TO1.2 Smart Device (SD) rev. C" I use the IOMux tool to configure UART3 on EIM_D24/25 pins. And in the source code to use UART3 as the debug uart. When I power up the board the Test Menu is displayed but my typed response is ignored. It appears as if the RX pin is not configured properly.

ラベル(2)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,705件の閲覧回数
YixingKong
Senior Contributor IV

Oswald

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 件の賞賛
返信

1,705件の閲覧回数
YixingKong
Senior Contributor IV

Oswald

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信