Can UART3 in the iMX6 SDK function as Debug Uart ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can UART3 in the iMX6 SDK function as Debug Uart ?

2,191 次查看
os
Contributor I

I have a board similar to the iMX6Q Sabre SDB. I have the debug serial port connected to UART3 (pins EIM_D24/25). I am running the "Platform SDK (1.1) for MX6DQ TO1.2 Smart Device (SD) rev. C" I use the IOMux tool to configure UART3 on EIM_D24/25 pins. And in the source code to use UART3 as the debug uart. When I power up the board the Test Menu is displayed but my typed response is ignored. It appears as if the RX pin is not configured properly.

标签 (2)
标记 (2)
0 项奖励
回复
2 回复数

1,662 次查看
YixingKong
Senior Contributor IV

Oswald

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 项奖励
回复

1,662 次查看
YixingKong
Senior Contributor IV

Oswald

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 项奖励
回复