Can IMX6UL run on Android?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can IMX6UL run on Android?

2,239件の閲覧回数
robinkwek
Contributor I

Hi,

Can i.MX6 UltraLite run on Android?

If yes, what is the memory size needed?

ラベル(2)
0 件の賞賛
返信
1 返信

1,432件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Robin

one can look at  porting Android for i.MX28 EVK (128MB)

http://markdingst.blogspot.com/2011_07_01_archive.html  

In general hw acceleration is mandatory for Android (note, UL has

not gpu), as some api's may require support for hw acceleration.

Without gpu only the basic UI may be usable.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信