@Before beginning I asked a similar question but it marked as answered without a real answer. (you can see it here Why nothing happens after "jumping to os image" in mfg tool? )
Hello all,
I have a sabre automative imx6 board MCIMX6xAICPU1 board. I don't know much about MFG TOOL. I did these steps.
1- connected the Debug UART DB9 to PC.
2-connected USB OTG to PC
3- inserted an empty (also with no partition) SD card to PC. ( We also tried with sd card on board, sd card on both pc and board, no sd card.)
4- Ran the MFG TOOL ( It saw the HID - compliant device)
5 - Press start
6- It loaded uboot, kernel etc.
7- It reached the "jumping to os image" state and did nothing else.
So can you tell me all steps one by one with answeing these questions?
Are usb connections right?
Where should I put the SD card? PC or board?
I downloaded L4.1.15_1.1.0_ga-mfg-tools.tar.gz as mfg tool kit from here SABRE|Automotive-Infotainment|i.MX6|NXP
Is it enough itself for installing linux on SD card and/or board?
How can I show correct .dtb file to mfg tool?
Please, don't mark it as answered before it really get resolved. Thanks from now.
sinanakman