I use i.MX6 dual in Linux and want to seperate tasks each cores.
Then is it possible to designate a core to excute codes?
For example, UART0 is running in core 0 and UART1 is running in core 1.
解決済! 解決策の投稿を見る。
Hi Jaehee
in Linux kernel takes all task for multiprocessing,
not leaving chance to change smth, you can not change its behaviour.
So trying to implement this seemingly simple task will bring you
to jungles of kernel programming
Linux Knowledge Base and Tutorial
However in SDK you will find such example, described in
Chapter 3 "Multicore Startup" document iMX6_Firmware_Guide.pdf
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
You could try "isolcpus” kernel parameter.
http://www.linuxtopia.org/online_books/linux_kernel/kernel_configuration/re46.html
You could isolate a CPU. Then a threat can be assigned to that core using cpu affinity to run the process on this core and IRQ affinity to freeze the isolated core of managing irq's.
Best Regards,
Luis
Luis,
Have you tried this?
I need to do this exact thing, but it doesn't quite work as I think it should...
I'm running with an iMX6Dual.
I want to put *everything* on core 0.
Then bring up one thread and set its affinity to core1.
So, in my kernel command line I add: ... isolcpus=1... to isolate core 1
And in the thread I run:
cpu_set_t mask;
CPU_ZERO(&mask);
CPU_SET(1,&mask);
sched_setaffinity(0,sizeof(mask),&mask);
to push it onto core 1; however, later I run:
printf("taskCore1 started (cpu=%d)\n",sched_getcpu());
and it tells me I'm on core 0.
Note if I don't include "isolcpus=1" on the command line, then this does
put that thread on core 1.
Any idea what's wrong here?
Ed
Hi Ed,
Try building this code: http://people.seas.harvard.edu/~apw/stress/
With standard parameters you should get:
./stress -c 4 &
top
CPU0: 99.2% usr 0.7% sys 0.0% nic 0.0% idle 0.0% io 0.0% irq 0.0% sirq
CPU1: 100% usr 0.0% sys 0.0% nic 0.0% idle 0.0% io 0.0% irq 0.0% sirq
CPU2: 100% usr 0.0% sys 0.0% nic 0.0% idle 0.0% io 0.0% irq 0.0% sirq
CPU3: 100% usr 0.0% sys 0.0% nic 0.0% idle 0.0% io 0.0% irq 0.0% sirq
With isolcpus=1
Mem: 57632K used, 708340K free, 0K shrd, 3512K buff, 15920K cached
CPU0: 100% usr 0.0% sys 0.0% nic 0.0% idle 0.0% io 0.0% irq 0.0% sirq
CPU1: 0.0% usr 0.0% sys 0.0% nic 0.0% idle 0.0% io 0.0% irq 0.0% sirq
CPU2: 100% usr 0.0% sys 0.0% nic 0.0% idle 0.0% io 0.0% irq 0.0% sirq
CPU3: 99.6% usr 0.3% sys 0.0% nic 0.0% idle 0.0% io 0.0% irq 0.0% sirq
And with :
taskset 2 ./stress -c 4 &
top
Mem: 58320K used, 707652K free, 0K shrd, 3784K buff, 15920K cached
CPU0: 0.0% usr 1.0% sys 0.0% nic 98.9% idle 0.0% io 0.0% irq 0.0% sirq
CPU1: 100% usr 0.0% sys 0.0% nic 0.0% idle 0.0% io 0.0% irq 0.0% sirq
CPU2: 0.0% usr 0.0% sys 0.0% nic 100% idle 0.0% io 0.0% irq 0.0% sirq
CPU3: 0.0% usr 0.0% sys 0.0% nic 100% idle 0.0% io 0.0% irq 0.0% sirq
In your case with 2 cores.
Best Regards,
Luis
This email and any associated attachments have been classified as
Freescale General Business
Freescale Internal Use Only
Freescale Confidential Proprietary
"All types of technical support (Schematic review, layout review, software review, hardware board and software) provided by Freescale Field application team are subject to Freescale's general Terms and Conditions unless superseded by a direct contract".
Thanks Luis,
once I realized the mistake I made (and fixed it), everything worked as expected.
Ed
Ok, nevermind, I'm a moron...
I had misplaced one line in the code.
If I actually had used the code that I show above it would have worked.
I add this comment instead of deleting the previous reply I made because it may be useful to someone else.
:-(
Hi Jaehee
in Linux kernel takes all task for multiprocessing,
not leaving chance to change smth, you can not change its behaviour.
So trying to implement this seemingly simple task will bring you
to jungles of kernel programming
Linux Knowledge Base and Tutorial
However in SDK you will find such example, described in
Chapter 3 "Multicore Startup" document iMX6_Firmware_Guide.pdf
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------