Can I decode 3840x1080P30 using Hardwre decoding function(it is called VPU).

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I decode 3840x1080P30 using Hardwre decoding function(it is called VPU).

ソリューションへジャンプ
4,077件の閲覧回数
hyungjunyoon
Contributor I

Hello.

I want to decode 3840x1080P 30frame/s(3840x1080p30) at i.MX6Q SabreSD Board. (Android Jellybean 4.2.2-1.1.0)

According to Maunal, I.MX6Quad/Dual can decode upto 1920X1080P 60frame/s.

So I think that it is possible, becase both have same bandwidth.

I tried to decode 3840x1080p30 Video, and It can be decoded but cannot use hadware decode function. so it is very slow (for only using software decoding).

Can I decode 3840x1080P30 using Hardwre decoding function(it is called VPU).

Please Let me know if anyone knows about the way.

Thank you.

Hyungjun Yoon

SiliconCube.co, Ltd

www.siliconcube.co.kr

ラベル(6)
0 件の賞賛
返信
1 解決策
3,741件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

It cannot be done by hardware, only by software but as you already saw, it will be painfully slow.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,742件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

It cannot be done by hardware, only by software but as you already saw, it will be painfully slow.

0 件の賞賛
返信
3,741件の閲覧回数
hyungjunyoon
Contributor I

thank for your help.

0 件の賞賛
返信
3,741件の閲覧回数
saurabh206
Senior Contributor III

Hi,

Which application you are using to decode this vector?

You can try with Default Gallery and check the logcat information. This will provide you more detail.

Thanks

Saurabh

0 件の賞賛
返信
3,741件の閲覧回数
hyungjunyoon
Contributor I

Default Gallery and Cactus Player were not able to decode the video.

I could only decode it at Mxplayer, but using software decoding. (it is very slow....)

0 件の賞賛
返信
3,741件の閲覧回数
saurabh206
Senior Contributor III

Hi,

Can you provide the logcat detail? Only this will be helpful...

There may be limitation in VPU for dimensions...or may be some error in OMXPlayer framework...

Thanks

Saurabh

0 件の賞賛
返信