Can I decode 3840x1080P30 using Hardwre decoding function(it is called VPU).

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can I decode 3840x1080P30 using Hardwre decoding function(it is called VPU).

跳至解决方案
4,090 次查看
hyungjunyoon
Contributor I

Hello.

I want to decode 3840x1080P 30frame/s(3840x1080p30) at i.MX6Q SabreSD Board. (Android Jellybean 4.2.2-1.1.0)

According to Maunal, I.MX6Quad/Dual can decode upto 1920X1080P 60frame/s.

So I think that it is possible, becase both have same bandwidth.

I tried to decode 3840x1080p30 Video, and It can be decoded but cannot use hadware decode function. so it is very slow (for only using software decoding).

Can I decode 3840x1080P30 using Hardwre decoding function(it is called VPU).

Please Let me know if anyone knows about the way.

Thank you.

Hyungjun Yoon

SiliconCube.co, Ltd

www.siliconcube.co.kr

0 项奖励
回复
1 解答
3,754 次查看
SergioSolis
NXP Employee
NXP Employee

It cannot be done by hardware, only by software but as you already saw, it will be painfully slow.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,755 次查看
SergioSolis
NXP Employee
NXP Employee

It cannot be done by hardware, only by software but as you already saw, it will be painfully slow.

0 项奖励
回复
3,754 次查看
hyungjunyoon
Contributor I

thank for your help.

0 项奖励
回复
3,754 次查看
saurabh206
Senior Contributor III

Hi,

Which application you are using to decode this vector?

You can try with Default Gallery and check the logcat information. This will provide you more detail.

Thanks

Saurabh

0 项奖励
回复
3,754 次查看
hyungjunyoon
Contributor I

Default Gallery and Cactus Player were not able to decode the video.

I could only decode it at Mxplayer, but using software decoding. (it is very slow....)

0 项奖励
回复
3,754 次查看
saurabh206
Senior Contributor III

Hi,

Can you provide the logcat detail? Only this will be helpful...

There may be limitation in VPU for dimensions...or may be some error in OMXPlayer framework...

Thanks

Saurabh

0 项奖励
回复