Can Connectivity

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can Connectivity

Jump to solution
2,923 Views
athul_am
Contributor II

Hi ,

I have a IMX6 ULL evk board with me . My understanding is that it has a CAN Capability.

Can someone let me know the connector to connect a DB-9 connector to the Board, also if the base image that comes with the box has CAN enabled if not how to enable it.

Thanks in Advance,
Athul

Labels (1)
0 Kudos
Reply
1 Solution
2,807 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello, 

If you are looking for the exact part number, is WF1250801200, but it appears is not longer in production.

You can refer to this link to see the pinout of the 9-pin D connector.

Alejandro_Salas_0-1727104403705.png

Best regards,

Salas.

 

View solution in original post

4 Replies
2,904 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @athul_am 

 

All i.MX 6 supports one CAN with the default device tree on i.MX 6SABRE-AI. Supports both CANs using the FlexCAN device tree but has a pin conflict with FEC. Supports with the default device tree on i.MX 6SoloX-SD, 7Dual SABRE-SD, 6Ultre Lite EVK, and 6ULL EVK. With the platform that supports the FlexCAN module, FlexCAN supports CANFD mode.

 

Also you can take a look to the table Table 42. FlexCAN Driver Files on IMX Reference Manual.

 

Also, the i.MX6ULL provides a CAN access through the J1201 port.

Alejandro_Salas_0-1726090008241.png

 

Best regards,

Salas.

0 Kudos
Reply
2,837 Views
athul_am
Contributor II

Hi @Manuel_Salas ,

 

If you cant provide me a Connector . Can you please let me know the use of each pin in the 8-pin port? like CAN0_H for which pin and CAN0_L for which pin etc.

 

Thanks,

Athul

0 Kudos
Reply
2,808 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello, 

If you are looking for the exact part number, is WF1250801200, but it appears is not longer in production.

You can refer to this link to see the pinout of the 9-pin D connector.

Alejandro_Salas_0-1727104403705.png

Best regards,

Salas.

 

2,893 Views
athul_am
Contributor II

Hi @Manuel_Salas ,

 

Thank you for the reply . I would like the connector to be used to connect the imx6ull board can port to the DB-9 Connector as the package of the board did not come with one included.

 

Thanks in advance,

Athul

0 Kudos
Reply