Camera video frame shift problem on IMX8MM CSI + NEXTCHIP N4 (NVP6324, NTSC)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Camera video frame shift problem on IMX8MM CSI + NEXTCHIP N4 (NVP6324, NTSC)

4,288件の閲覧回数
yulsangkim
Contributor I

This is a problem that occurred during the NEXTCHIP N4 (NVP6324, CSI) video decoder test on IMX8MM.

It uses mx6s_capture.c and mxc_mipi_csi.c drivers based on Linux 4.14.78-GA1.0.0 version.

There is a problem that the captured video frame shifts like the attached file.

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

4,215件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yulsang

Linux 4.14.78 is old kernel and not more supported, suggest to try

latest for example L4.14.98, may be useful to look at

MIPI Camera Frame corruption in IMX8MM when MIPI_DOUBLE_CMPNT and MIPI_YU_SWAP is enabled in CSI_CSI... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,215件の閲覧回数
yulsangkim
Contributor I

Hi 

Fixed the problem of left rolling by setting FCC bit of CSICR1 register to 0.

Thank you!

0 件の賞賛
返信