Camera for a MCIMX6Q-SDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Camera for a MCIMX6Q-SDB

1,617件の閲覧回数
maxschrake
Contributor I

Is it possible to use the camera the Raspberry PI uses for the MCIMX6Q-SDBs camera connector ?

And if not what cameras can i use ?

Greetings Max

0 件の賞賛
返信
2 返答(返信)

1,472件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

If you are referring to this one:

http://www.raspberrypi.org/products/camera-module/

then yes, it is supported, as Saurabh said, you can use the MIPI and CSI interfaces (as well as USB).

You would need to develop your own driver for it though.

0 件の賞賛
返信

1,472件の閲覧回数
saurabh206
Senior Contributor III

Hi Max

IMX6 supports MIPI and CSI camera interface.

0 件の賞賛
返信