Camera flow in linux-3.10.53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Camera flow in linux-3.10.53

1,892 Views
chandrasekharma
Contributor III

Hi all,

I am new to imx6 sabresd board and my device running in Android-5.0.2 with linux kernel 3.10.53.

Please help me to find camera flow in linux kernel 3.10.53.

My first doubt from where i need to start to find camera flow driver whether i need to read any datasheets or any material?

So please help me how to find camera driver files in linux-3.10.53?

Thanks in advance

Labels (3)
0 Kudos
Reply
1 Reply

1,771 Views
igorpadykov
NXP Employee
NXP Employee

Hi chandrasekhar

linux kernel 3.10.53 camera drivers are described in attached Linux

Manual Chapters 6,20, for camera flow one can look at presentation on

A Deep Dive into Image Processing for i.MX 6 Se... | NXP Community

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply