iMX6Q : How to work a software reset ( set SRC_SCR register ) ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6Q : How to work a software reset ( set SRC_SCR register ) ?

ソリューションへジャンプ
1,100件の閲覧回数
koichisakagami
Contributor II

Dear community,
I am checking a SRC_SCR register coreX_rst field. (X is 0,1,2,3)

In the case of setting a coreX_rst field , does the reset process begin immediately ?

Or , after performing any process , does the reset process subsequently begin ?

Best Regards,
Koichi Sakagami

ラベル(1)
0 件の賞賛
返信
1 解決策
890件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  timings for the secondary CPU reset are not specified, since this

is mainly software, not hardware, process.

"Once the bits are set, the corresponding core is released from its reset state,

and it executes the boot ROM (at 0000 0000h). The boot ROM determines if it
is a secondary core and uses the persistent bit registers to determine what to
execute next."

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
891件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  timings for the secondary CPU reset are not specified, since this

is mainly software, not hardware, process.

"Once the bits are set, the corresponding core is released from its reset state,

and it executes the boot ROM (at 0000 0000h). The boot ROM determines if it
is a secondary core and uses the persistent bit registers to determine what to
execute next."

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信