Camera flow in linux-3.10.53

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Camera flow in linux-3.10.53

1,923件の閲覧回数
chandrasekharma
Contributor III

Hi all,

I am new to imx6 sabresd board and my device running in Android-5.0.2 with linux kernel 3.10.53.

Please help me to find camera flow in linux kernel 3.10.53.

My first doubt from where i need to start to find camera flow driver whether i need to read any datasheets or any material?

So please help me how to find camera driver files in linux-3.10.53?

Thanks in advance

ラベル(3)
0 件の賞賛
返信
1 返信

1,802件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi chandrasekhar

linux kernel 3.10.53 camera drivers are described in attached Linux

Manual Chapters 6,20, for camera flow one can look at presentation on

A Deep Dive into Image Processing for i.MX 6 Se... | NXP Community

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信