Camera Kernel module load order

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Camera Kernel module load order

ソリューションへジャンプ
7,842件の閲覧回数
dennis3
Contributor V

I'm working on bringing up a mipi camera on the imx8mp board.   Android 11 2.2.0 is using GKI kernel config, which means all the custom modules we use for our board are compiled as .ko objects.  Even if I select to compile them as built in modules, the build process modifies the .config and creates kernel modules anyway.  But I think whether it is built in or external isn't the most important issue.

The problem is, that the imx8_media_dev module is loading before my camera module.  So when that module loads, it isn't finding any cameras.  Here is the output:

[    1.304994] mxc-isi 32e00000.isi: mxc_isi.0 registered successfully
[    1.338977] mx8-img-md: Registered mxc_isi.0.capture as /dev/video2
[    1.351040] unregister ISI channel: mxc_isi.0

After unregister, there is no longer a /dev/video2 device.

My camera kernel module loads slightly thereafter and never does anything because no video links are created.

The Basler kernel module loads before the imx8_media_dev module and if we're using that camera, video links are created and all works as expected.  In addition, if I manually unload the imx8_media_dev module after boot, and manually load it again (having already loaded our camera driver), the video links are created properly and our camera can work.

So I seem to be missing something in the build process or setup of our system that ensures our camera driver loads before imx8_media_dev.  Can someone suggest how this is accomplished?  I've placed my kernel module in the vendor_ramdisk, same location as the Basler kernel module is located but that doesn't seem to do the trick.

 

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
7,608件の閲覧回数
dennis3
Contributor V

In case anyone comes across this, it seems the module load order can be controlled.  We just needed to put our camera module after the appropriate CSI modules in SharedBoardConfig.mk.  The CSI modules can then load first and the camera module does cause the appropriate channels to be created.

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
7,609件の閲覧回数
dennis3
Contributor V

In case anyone comes across this, it seems the module load order can be controlled.  We just needed to put our camera module after the appropriate CSI modules in SharedBoardConfig.mk.  The CSI modules can then load first and the camera module does cause the appropriate channels to be created.

0 件の賞賛
返信
7,787件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

did you try the demo images? what board do you use? nxp board or customized board? I haven't tested this version before, let me reproduce this

0 件の賞賛
返信
7,785件の閲覧回数
dennis3
Contributor V

The demo image works fine with the Basler camera demo.  (Variscite Development Board).

Only our custom camera driver (which is very similar to Basler) loads AFTER media-dev instead of before.. causing the issue.

I have worked around the issue by modifying the gki_config to have built in mipi and csi drivers as well as our camera driver and this allows our camera to load before media dev and establish a camera media channel.  This doesn't seem to be the correct solution though as it would be more desirable to not modify the default gki_config for the board.

0 件の賞賛
返信
7,831件の閲覧回数
artsiomstaliaro
Contributor IV

Did you add I2C handle of the camera? Which camera are you using?

0 件の賞賛
返信
7,817件の閲覧回数
dennis3
Contributor V

We use a custom camera and ISP.  The driver is very similar to the OV5640 or Basler sample cameras though.

I'm not sure what you mean by an I2C handle.  This is our v4l subbev init code though:

    v4l2_i2c_subdev_init(sd, client, &camera_subdev_ops);

    sd->flags |= V4L2_SUBDEV_FL_HAS_DEVNODE|V4L2_SUBDEV_FL_IS_I2C;
    sd->entity.function = MEDIA_ENT_F_CAM_SENSOR;
    camera_data.pad.flags = MEDIA_PAD_FL_SOURCE;
    sd->entity.ops = &camera_sd_media_ops;
    retval = media_entity_pads_init(&sd->entity, 1, &camera_data.pad);
    if (retval<0) {
        dev_err(&client->dev, "media entity pad init fail: %d", retval );
        return retval;
     }

    retval = v4l2_async_register_subdev_sensor_common(sd);
0 件の賞賛
返信
7,773件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

which camera do you refer to? basler or ov5640, they use the different path

0 件の賞賛
返信
7,768件の閲覧回数
dennis3
Contributor V

Our camera driver is more similar to the ov5640 driver.

0 件の賞賛
返信
7,739件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what source code do you change? pls share your dts file with me

0 件の賞賛
返信