Camera Driver Update

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Camera Driver Update

1,812件の閲覧回数
Cococarbine
Contributor II

Hello,

I currently have a 8m nano evk with an OnSemi AS0260 camera connected to the Mini-SAS port using a custom connector board.  I am able to create a bootable SD card using the default evk linux (full) image provided by NXP.  I believe the next steps are to modify or add a driver for the camera.  What is the procedure, or where are the files that I need to modify to communicate with this camera?

ラベル(1)
0 件の賞賛
返信
1 返信

1,803件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信