Camera Driver Update

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Camera Driver Update

1,194 次查看
Cococarbine
Contributor II

Hello,

I currently have a 8m nano evk with an OnSemi AS0260 camera connected to the Mini-SAS port using a custom connector board.  I am able to create a bootable SD card using the default evk linux (full) image provided by NXP.  I believe the next steps are to modify or add a driver for the camera.  What is the procedure, or where are the files that I need to modify to communicate with this camera?

标签 (1)
0 项奖励
回复
1 回复

1,185 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复