Camera Driver Update

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Camera Driver Update

1,845 Views
Cococarbine
Contributor II

Hello,

I currently have a 8m nano evk with an OnSemi AS0260 camera connected to the Mini-SAS port using a custom connector board.  I am able to create a bootable SD card using the default evk linux (full) image provided by NXP.  I believe the next steps are to modify or add a driver for the camera.  What is the procedure, or where are the files that I need to modify to communicate with this camera?

Labels (1)
0 Kudos
Reply
1 Reply

1,836 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply