Calibration of i.mx6 32bit bus DDR3 with 2 CS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Calibration of i.mx6 32bit bus DDR3 with 2 CS

2,193件の閲覧回数
zc_tee
Contributor III

Hi all,

i am trying to do calibration of the i.mx6 32bit bus DDR3 RAM with 2 Chip Select using the DDR Stress Test tool

My calibration always return failed if i tried to calibrate both CS together (select from the selection that prompt in the DDR Stress Test tool)

If i calibrate CS0 only, it will success.

I come across this article:

Re: 32bit bus width memory with 2 cs in IMX6Q

I tried to modified the MDMISC[CALIB_PER_CS] bit in the .inc file, but how do i confirm whether it's calibrating CS0 or CS1?

Is this method applicable with using the DDR Stress Test tool?

Thank you.

Regards,

Tee

ラベル(2)
タグ(2)
0 件の賞賛
返信
5 返答(返信)

1,771件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please use the recent DDR stress tool i.MX6/7 DDR Stress Test Tool V2.40

For it : "You can select 0 for CS0 and ALL for both CS0 and CS1. There is no CS1 option."

Also, from section 5 )Calibration and Chip Selects) of app note AN4467 (i.MX 6 Series
DDR Calibration
) : "Should both chip selects be populated, it is an absolute must that the
memories populated on CSD1 are “mirrored” with the memories populated on CSD0, as both
CSD share the same delay line register set during normal DDR operation"

http://www.nxp.com/files/32bit/doc/app_note/AN4467.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,771件の閲覧回数
zc_tee
Contributor III

Hi Yuri,

Just for confirmation, does it means that i cannot calibrate the CS1 ONLY, even if i set the MDMISC[CALIB_PER_CS] bit to 1?

Thank you.

Regards,

Tee

0 件の賞賛
返信

1,771件の閲覧回数
Yuri
NXP Employee
NXP Employee

The Stress tool is not intended for CS1 calibration.

Regards,

Yuri.

0 件の賞賛
返信

1,771件の閲覧回数
zc_tee
Contributor III

Hi Yuri,

If that is the case, can you recommend any tool that we can use to calibrate CS1?

Thanks.

Regards,

Tee

0 件の賞賛
返信

1,771件の閲覧回数
Yuri
NXP Employee
NXP Employee

We do not have such tool if memories populated on CSD1 are NOT “mirrored”
with the memories populated on CSD0.
Sorry.

Regards,

Yuri.

0 件の賞賛
返信