CVBS output PAL format is cropped

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CVBS output PAL format is cropped

4,093件の閲覧回数
flto
Contributor I

Hi,

I try to output video on a CVBS display (from iMX53 with linux-2.6-imx-rel_imx_2.6.35_11.09.01 kernel from Freescale).

The display accepts PAL video format, so I use this kernel command line arguments :

video=mxcdi1fb:TV-PAL tve ldb=off

Thus my /dev/fb0 is displayed on the screen... but not entirely !

The image is cropped by about 30 pixels (left and right) and 15 pixels (top & bottom) [This is a rough estimation]

With an old TV, the image is cropped almost the same (but not exactly) and not cropped top and bottom when in 16:9 mode.

Does anyone know about CVBS, and has an idea why this happens ?

Here is fbset output:

$ fbset

mode "720x576-25"

        # D: 13.500 MHz, H: 15.625 kHz, V: 25.000 Hz

        geometry 720 576 720 1728 32

        timings 74074 132 11 22 26 1 1

        accel false

        rgba 8/16,8/8,8/0,8/24

endmode

ラベル(4)
0 件の賞賛
返信
5 返答(返信)

3,328件の閲覧回数
Kanstantsin1
Contributor III

So, I have resolved it in such way:

I fill only 656x544 at the center of the 720x576 screen. And leave black fields.

BTW: I have found that: different devices show different region of the image. For example PC-capture-card shows almost whole 720x576 image.

0 件の賞賛
返信

3,367件の閲覧回数
Kanstantsin1
Contributor III

Hi @flto Have you resolved the issue?

I have stumbled to the same problem and don't know how to solve it.

Can you share with your way to solve?

0 件の賞賛
返信

3,851件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Can you please share what pins, or configuration you are using for the CVBS output,? are you using the TV Encoder output?

0 件の賞賛
返信

3,367件の閲覧回数
Kanstantsin1
Contributor III

I have the same problem. ADV7391.

BT656-PAL configuration. But I see the cropped video even when I switch on COLOR-BAR-PATTERN

0 件の賞賛
返信

3,851件の閲覧回数
flto
Contributor I

Here is related schematics :

tve.png

0 件の賞賛
返信