CST to create signature for digest from HASH of firmware image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CST to create signature for digest from HASH of firmware image

974件の閲覧回数
LanBui
Contributor I

Dear NXP supporter,

We are developing security boot solution for our product using I.MX8DQX device. However, from: AN12312.pdf document, we understand that signature is calculated from container header (container header as signed data) and not form FW image as following figure:

LanBui_0-1630400971438.png

Is this possible to change to calculate HASH521 from FW image and used as input for signaure? 

ラベル(1)
0 件の賞賛
返信
1 返信

961件の閲覧回数
Yuri
NXP Employee
NXP Employee

@LanBui 
Hello,

   The container signature, shown on the picture, is verified against the SGK key
certificate, which is then verified against the SRK table. Images are not checked
at this stage. But the images are checked / authenticated, using the SGK, later,
as shown on Figure 2 (Secure boot flow overview)  of the app note.

  

Regards,
Yuri.

0 件の賞賛
返信