CSI0 test mode does not work with input channel CSI->IC->MEM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CSI0 test mode does not work with input channel CSI->IC->MEM

1,153 Views
RobbieJiang
Contributor IV

Hi,

I would like to have CSI0 work in test mode on my Mx6q sabrelite board.

But by now, I can only capture data through input channel 1, that is ,

from CSI directly to memory.  And no data can be captured through input channel 0,

which is CSI-->IC-->MEM.

So does csi in test mode  only work with input channel CSI-->MEM?

Labels (2)
0 Kudos
Reply
1 Reply

976 Views
joanxie
NXP TechSupport
NXP TechSupport

what test mode do you mean? if you mean the unit test, mxc_v4l2_capture.out is for csi-> mem, mxc_v4l2_overlay.out is for Direct previewing the camera to SDC foreground

0 Kudos
Reply