CSI parallel camera using mx6s_capture.ko on imx6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CSI parallel camera using mx6s_capture.ko on imx6Q

2,216 Views
lampo
Contributor I

I am porting parallel camera(mt9v034/mt9v032) driver on imx6Q , and the driver for imx6Q(mxc_v4l2_capture) is old using v4l2_int_device, while the mt9v034.c(provided by cmos sensor corp) using v4l2_subdev.

There are two folders in /drivers/media/platform/mxc, the capture driver is meant for platforms having/using the IPU (i.MX6Q, i.MX6QP, i.MX6DL etc...). Whereas the subdev is targeting the other platforms (i.MX6SL, i.MX6SX, i.MX7 etc...).

I want to know, if I don't need the IPU, can I just use mx6s_capture.ko and mt9v034.ko on imx6Q ? Are there any extra porting I should do ?

Labels (1)
0 Kudos
Reply
2 Replies

1,657 Views
igorpadykov
NXP Employee
NXP Employee

Hi glb

mx6s_capture uses CSI/PxP modules, not present in i.MX6Q

so seems this is not possible.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,657 Views
lampo
Contributor I

is there any parallel camera driver using v4l2_subdev interface  on imx6Q?    if not, did I have to modify mt9v034.c back to v4l2_int_device interface, or what can I do ?   thanks a lot!

0 Kudos
Reply