CSI connection in i.MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CSI connection in i.MX6DL

1,495 Views
ko-hey
Senior Contributor II

Hi all

I have a question about CSI input connection with i.MX6DL.

My customer want to use CSI in following setteing.

・YUV422 16bit 1cycle

However, they use only "Y" data in their system.

So they plan to connect pins of "UV" data to the GND.

Is it appropriate connection ?

Ko-hey

Labels (5)
Tags (2)
0 Kudos
Reply
3 Replies

1,398 Views
b36401
NXP Employee
NXP Employee

You can pull down "UV" pins. It is possible.

However please note that in case of zeroing U and V you get green not white.

I mean you get monochrome, but black-green, not black-white pictute.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,398 Views
ko-hey
Senior Contributor II

Hi Victor

Thank you for reply.

How about Pull-up ?

Is it better than connecting to GND ?

Ko-hey

0 Kudos
Reply

1,398 Views
ko-hey
Senior Contributor II

Hi Victor

On second though, there are no recommendation about the connection in this case.

Because it depends on user's use case.

Is my though correct ?

Ko-hey

0 Kudos
Reply