CSI camera HW module example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CSI camera HW module example

2,233 Views
AdCmo
Contributor III

All,

We are trying to do a demo CSI implementation using the i.MX53 QSB.

We would like buy a simple stand alone camera module that we can

rewire externally to connect directly to an existing i.MX53 CSI header.

Anyone aware of a such a cheap module out there we can buy?

It must have some driver support in i.MX53 LTIB or ideally has been

used before by someone in the i.MX community.

Looking forward to your suggestions,

Ad.

-------------------

0 Kudos
Reply
3 Replies

2,050 Views
AdCmo
Contributor III

Roy,

Thanks, I ended up going with these guys: http://www.bestelecs.com/

via their ebay account:

http://www.ebay.com/itm/ws/eBayISAPI.dll?ViewItem&item=270752614779&ssPageName=ADME:L:OU:US:1123

Pretty responsive, helpful and fast shipment considering coming out of China.

Still designing the daughter card for it for the i.MX53QSB expansion header.

Unless if Freescale had an easily adaptable daughter card handy of course :(

Ad.

---------------------

0 Kudos
Reply

2,050 Views
roybunce
Contributor II

I'm looking for the same thing and found this:

http://www.aliexpress.com/store/404311/210037410/CAMERA-MODULE.html

Not tried it yet though!

Roy

0 Kudos
Reply

2,049 Views
AdCmo
Contributor III

All,

Any quick comment/reference?

I have been googling around and I still can't find where to reliably buy an OV3640 camera module, for example :(

Or an alternative that also supports the serial data interface.

I just want something ready made that I can custom connect to the i.MX53 QSB header.

Thanks,

Ad.

0 Kudos
Reply